This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: How to determine switching frequency

Guru 12805 points
Part Number: TPS61099
Other Parts Discussed in Thread: TPS61299, , TPS61033

Hi, 

We are newly considering TPS61099 or TPS61299. These are types with variable switching frequency. Could you tell me in what range it can be changed? Or could you please tell me the formula?
In particular, we are concerned about other circuits being affected by the effects of low switching frequencies during light loads (such as when there is no load).

■Terms of use
・VIN: 3V
・VOUT: 3.3V
・Iout: 50mA

Thanks,

Conor