This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552882-Q1: maximum current capability

Part Number: TPS552882-Q1

Hi Experts,

on the website the max. output current for the device is mentioned to be 6.35A. What determines this current limit/capability? I did not find an explanation in the datasheet.

BR Simon

  • Hi Simon,

    Since this is an converter part, the device maximum output power depends on the input voltage/output voltage condition. I would suggest refer to datasheet efficiency curve.

    Or you can let us know the application input and output parameter, we could give you some comment.