This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3410: LM3410XQMF/NOPB

Part Number: LM3410

Hi,

I am considering using LM3410XQMF/NOPB LED driver in my project to drive a LCD backlight (which will be requiring 19.2V, 240mA).I am giving 5V as input voltage to the LED driver IC. I am planning to give 100% PWM to DIM pin for 24 LED Circuit. Please let me know whether I can use this IC for my requirement. Also, suggest if any alternate which is compatible for (input voltage=19.2V, Current I=240mA) and (input voltage=10.5V, Current I=200mA).

Thanks & Regards,

Jothi Mathi.