Other Parts Discussed in Thread: LM5032, UCC28C53, LM5021, UCC29002, TPS25961, LM5050-1
Hi
I'm going to develop SMPS for the server as below.
Please recommend a solution.
There are two models.
-SPEC-
1. AC/DC model (288W)
① INPUT : 90Vac ~ 264Vac 50/60Hz (45~66Hz)
② output (288W)
-48V 3.5A(MAX 168W)
+12V 10A(MAX 120W)
2.DC/DC model (120W)
① INPUT : -38Vdc ~ -58Vdc
② output
+12V 10A(MAX 120W)
*Required Features
① Power supply redundancy mode (N+1)
②Hot Swap
③ Load share
Thanks