This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2065: pin 8 (OUT) floating

Part Number: TPS2065


Hi 

  My customer uses AP2191 and I'd like to replace it. TPS2065DGN is almost P2P, except pin 8 (OUT). AP2191 pin 8 is NC, floating on layout.

if 1A is good enough, may I put TPS2065 pin 8 in floating? Assumed it should be fine for 1A output.

  • Hi Alan,

    Floating the Pin8 will not impact the output function, but the pin 6, 7and 8 work together to support 1A continuous current, if you don't use the pin8, the max continuous current should decrease to 0.66A, that should be ok.Thank you.

    Best Regards,

    Kuno