Hi Team,
TPS2419 controls the combination of two 12V power supplies, which are connected to the NMOS of VISHY externally. Rds=0.0005Ω. RSET is set to 150K. When the two power modules are powered on at the same time, the TPS1249 will work alternately, and the power consumption is about hundreds of thousands of watts. Customer wants to know how to adjust to keep both working?
Regards,
Annie