This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2663: Recommended replacement for the LM2662/3

Guru 10890 points
Part Number: LM2663
Other Parts Discussed in Thread: LM2662, LM2660, TL7660, MAX660

Hello,

Currently, the LM2662/3 is in LTB state.

The P2P products with the same package that I found when ignoring the usage specifications and the number 1 PIN function are as follows.

 - TL7660, MAX660, LM2660

Q1 ) Considering only the package, are there other products besides the 3 devices I found?

Q2 ) Please recommend the most suitable replacement when not considering the P2P package.

Thank you.

JH