Part Number: BQ25896
Other Parts Discussed in Thread: BQ25895
Hi,
In my circuit 12V is the Vin that is used step down to 5V and then 3.3V for powering the microcontroller and other peripherals. Also 12V is used to charge the battery.
Whenever the 12V is absent the booster circuit automatically boost the battery voltage to 5V.
I selected the BQ25896 IC for battery charging and boosting. While going through datasheet. I have a doubt in boost mode of BQ25896 and BQ25895 integrated Buck boost battery charger IC.
As per datasheet Boost mode enable in
1. BAT above BATLOWV
2. VBUS less than BAT+VSLEEP (in sleep mode)
3. Boost mode operation is enabled (OTG pin HIGH and OTG_CONFIG bit =1)
4. Voltage at TS in range
5. After 30 ms delay from boost mode enable
So my doubt is how the microcontroller give i2c command to buck boost IC when 12V is not present and if it's 30ms taken for after command in the mean time board will goes to off.
If you can suggest an standalone buck boost having Single Li-ion battery charge current 1 to 2A and discharge current 2A.