My customer has two applications for the LMR38010-Q1 where the output voltages are 20V and 30V. They are looking at using an electrolytic capacitor output instead of ceramic capacitors because the ceramic caps derate so much with DC bias. The data sheet defines a minimum output capacitance (15μF after derating – page 19, Figure 9-1, using 24V out). The assumption is the table assumes ceramic capacitors are used. The issue with an electrolytic capacitor is the cap esr is much higher than a ceramic cap. So two questions:
1.) Is there addition information or equations available for the LMR38010-Q1 so we can see how higher ESR output capacitors impacts stability?
2.) Assuming some ceramics are required, do we have a formula or procedure for mixed electrolytic & ceramic operation?
Thanks!