Other Parts Discussed in Thread: TPS565247, TPS565208
Hi,
We would like to get recommendation about the DC-DC converter parts. Our requirements are below.
- Vin = 5V
- Vout = 1V
- Output ≧ 4A
- Fixed average current limit <8A
Note that "valley current" limit of <8A is not sufficient for our use case, but If its low enough, it might be good when appropriate frequency and inductor are selected.
We are considering TPS564257 for now but we would like to know if there are better parts available.
Best regards,