This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2663: Priority Power MUX Operation

Part Number: TPS2663

Hi,

Would it be possible to use the architecture proposed on page 36 of the datasheet for Priority Power MUX Operation but connecting the dvdt pin output of the primary efuse to the SHDN# pin of the secondary efuse through an N-channel MOSFET? Is there any problem this can cause or do you see any problem?

  • Hi Mikel,

    That is also possible. I think only difference is that recovery from OVP is fast as compared to SHDN so when primary goes away and secondary comes up VOUT droop will be less in case of OVP based approach.

    Regards

    Kunal Goel