Hi,
My switch regulator keeps burning at the VIN net and i'm trying to understand why.
The input us under 24v and I'm trying to achieve 3v on the output.
I followed the data sheet but don't understand what i am missing. bellow is my schematic.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My switch regulator keeps burning at the VIN net and i'm trying to understand why.
The input us under 24v and I'm trying to achieve 3v on the output.
I followed the data sheet but don't understand what i am missing. bellow is my schematic.
Hello
You may have some kind of voltage transient on your input supply.
Try to capture the input voltage when the device becomes damaged.
You may need more input capacitance in order to damp out any overvoltage
spikes on the input.
Is the device damaged during start-up, or during some other kind of test ?
Can you provide images of your PCB layout.
Thanks
Hello
1. In general the components should be placed closer to the IC.
2. A ground plane flood on the top layer should be used; as well as the bottom plane.
3. Cinx, C4,C5, C6 should all be as close to the device as possible.
4. Note that the data sheet recommends 4.7uF on the input.
5. Cboot should be close to the device and connected with short wide traces.
6. The feedback components should be connected directly to the output capacitor.
7. In general some ceramic output capacitance is needed on the output, depending
on the ESR of the aluminum output capacitor.
8. In general you will need to follow the PCB layout example in the data sheet
as closely as possible.
Thanks
I appreciate your help Frank. How about this? I added 2 x 4.7uF and 1 x 0.1uF input capacitors per the data sheet (Section 9.2.2.6).
My input will be 24v so i used 50v for each 4.7uF.
I tried to move the parts as close a possible while still allowing me space to solder the IC.
Added additional ground plane under the IC and more VIAs.
Hello
OK
I think you will also need to check that the input voltage is not
overshooting when you apply your input supply.
This could be caused by long leads from the input supply to the regulator.
Thanks