This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggested LiPo battery Charging IC

Other Parts Discussed in Thread: BQ25616, BQ24073

Hello Community,

I am working on the Quectel MC-60 GSM module. 

the GSM module must be powered by a micro USB interface & LiPO battery of 1000-2000mAh.

For that, I need the specific charging IC with the following features.

1, Charging IC input voltage is as per the micro USB interface standards & Max input current is up to 3Amp.

2. Charging IC has no external configuration interface (UART/I2C) & the charging current must be controlled by the external RC circuit. (charging current may vary from 500mAmp to 1Amp)

3. Status indication for charge & discharge,

4. Auto Cut-OFF on a full charge.

5. Auto Cut-OFF to prevent over-discharge.

Will you please help me to find the best cost-effective solution suitable for my kind of application?

Regards,

Shiv Patil.