With the circuit of TPS54561 as below A problem occurred during use
[Problem]
- SW(No.9 pin) <-> gnd short
- If you remove the tps54561 during repair, The circuit of the input/output is normal.
input/Output specifications are as follows:
1. input: SMPS 48V@20A
2. Output(Load): 12V@3~4A
Q-1. Are there any examples that would cause the same problem as now?
Q-2. Are there any conditions that exhibit the same symptoms as the problem?