Hi,
My questions are related to the BQ34Z100-G1 device.
I finished succesfully the learning process according to Ti documents. These are my questions:
1) When the learning is finished, the QMAXCELL0 has a value similar to the nominal cell capacity, but after working for some time this value is dropped to a very low value. Is it updated this parameter along the working life of the device, or it has correct value only just after the learning is finished? In all cases, the FCC I get (full charge capacity) is correct.
2) the STATIC_DF_CHKSUM command is not working. I get the value 0x0004 value. How can I get a dataflash checksum value in order to check the correct static flash parameter values?
3) What is the function of Charge Hys V shift value? is it correct to have a value of 1000mV?. Recommended values?
4) What is the function of DODatEOC Delta T? is it correct to have a value of 20? Recommended values?
5) What are updated parameters when a Reset command is sent? can be an update of SOC value? Related to this, when is it required to send a reset to the gas gauge along the system lifetime?
NOTE: my desing is a 8s2p LIFEPO battery pack. Attached is a gg.csv file
Regards