This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27714EVM-551: Using TI evaluation module for constant power control operation.

Part Number: UCC27714EVM-551
Other Parts Discussed in Thread: UCC28950, , PMP8740

I want to use UCC27714EVM-551 TI evaluation module as a constant power controlled Phase Shifted Full Bridge (PSFB), using the UCC28950 controller card provided with it.

I want suggestions on how to use the this evaluation module for the same as per following requirement:

  • Vout = 20-30V
  • Case 1) Pout  = 300W (constant & controlled using the UCC28950 controller card provided)
  • Case 2) Pout  = 100W (constant & controlled using the UCC28950 controller card provided)
  • This output will be fed to another converter which is supplying a pulsed load.

My aim is to use this evaluation module to work in Average Current mode control to process constant power at any instant with an output voltage which can be allowed to vary around 20-30V as per the load variation.

Can you suggest me how should I use/modify the controller for this operation?

Thanks,

Gaureej