Dear Frank, Dear Carol, good morning
Please answer:
1) When I choose an alternate out capacitor in WEBENCH and I create a "custom part", then the capacitance value and ESR are enough to correctly determine the phase margin parameter?
2) What does this mean: - "derated Cap per Cap" ? For example I use two capacitors of 100 microfarads each, then I must type "100" or "200"? I think "100", since I type quantity 2.
3) ESR per Cap - it is the ESR of one Cap (for example 50 mOhm). If I use two caps, then I must type "50" or "25"? I think "50", since I type quantity 2.
4) I made calculation, please see "WBdesignLM2596_1" and I want to create a custom out cap. I use two cap 100 microF, 150 mOhm and I see warning, please see "593D107X9020E2ETE3" file.
Then I click "SAVE" (100 microF,150 mOhm, two caps) and I get - please see "WBdesignLM2596_2". I understand, that at first the program "does not see" the fact that I installed not one capacitor, but two. And then, when calculating, WEBENCH sees that are two capacitors?
QUESTION: Can I assume that everything is fine? Or not? Phase margin parameter in both cases is within the allowable range.
5) Please remind me what is the maximum allowable value of the Phase margin parameter?
TIA
Vladimir Naumenkov