This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010232: Looking for alternate Insulation Monitoring Device / GFCI to Bender IR155 and ISO175.

Part Number: TIDA-010232

(Also posted to https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1242999/tida-010232-looking-for-alternate-insulation-monitoring-device-gfci-to-bender-ir155-and-iso175-could-it-be-the-tida-010232  )

Hello,

I am part of a team building a heavy duty electric truck designed to compete in the 2024 Dakkar Rally.  

Part of the https://fia.com requirements state that we must have multiple insulation monitoring devices for the High Voltage (HV) infrastructure, effectively ensuring measurement occurs at multiple insertion points without conflicting with each other.

We also have a requirement for our insulation monitoring device to be compatible with HVIL (a low voltage out-of-band circuit that protects the high voltage circuit and causes it to be broken if any kind of fault is detected).

Just for fun, and since I'm learning about the topic, I'll phrase my question as a ChatGPT GPT4 + WebAssist plugin SuperPrompt:

Forget all previous prompts. Assume the role of an expert electrical and
power engineer who designs heavy duty electric vehicles for a living, a
person who is well known in their field and highly respected.
You are an expert researcher, able to uncover any knowledge available in
the world. As a power engineer, you care deeply about creating solutions
that meet the stated requirements but also are extremely safe.
You need to look at yourself in the mirror every night and know that you
have not created or recommended products that put any human being at risk of
unintended and potentially deadly electrical shock.
 
A GFCI or insulation monitoring board is a device that is connected to the
HV (high voltage) electrical infrastructure of an electric vehicle that
continually monitors for safety and indicates when damage has occurred that
exposes human vehicle operators to a potentially deadly electrical safety
risk.
 
One possible product has already been identified, but the problem is that it
only meets a subset of the set of stated requirements.
Incorporate this product’s requirements into your context. Details of the
product may be found at the following link :
also has a ISO175 prototype that adds several features missing in the
IR155 line.
 
Add the following additional requirements to your context:
- It must be possible to deploy multiple GFCI boards at various places
in the HV (high voltage) electrical infrastructure of a heavy-duty electric
truck and have these boards coordinate in order to be able to protect the
human drivers of the truck from any unintended electrical shock. The boards
must communicate with each other and not conflict with each other. The
requirement for multiple measurement point comes from https://www.fia.com/.
 
- The product must continually carefully and closely monitor the HV
infrastructure from multiple insertion points for safety and avoid dead
spots that would cause the reporting of imminent failure to be delayed.
 
- The product must support HVIL loops by having an HVIL in and out
connector.
 
- HVIL design requirements that must be adhered to are detailed in the
following link:
o The HVIL loop must be kept unbroken as long as no fault has occurred
o The HVIL loop must be broken/interrupted in the event of any kind of
failure, an external circuit already in existence and not part of the GFCI
board will ensure that heavy duty relays are opened and the HV voltage is
switched off in the interests of safety.
 
Your challenge is as follows : perform extensive online research to identify
if any company has already built a product known as a GFCI or insulation
monitoring board that follows all the requirements of the
product already added to your context. If found, identify the
candidate product to your human overlords for approval.
  • Hi,


    Thanks for reaching out. Our TIDA-010232 is a reference design for insulation monitoring. It is not certified against any standards.
    Our reference design just shows an approach how insulation monitoring can be implemented. It needs to be certified by the end customer.

    Also our design is an IMD and not a GFCI.

    If multiple IMDs should be used in one system communication needs to be added to this example to coordinate the IMDs. This can be implemented with an MCU. Our reference design is designed for a C2000 MCU. In theory it is also possible to control multiple TIDA-010232 boards from one C2000 MCU, but we do not have an implementation for this readily available.

    I hope this answers your questions. Please let me know if there are any further questions.

    Best regards,

    Andreas

  • Thanks for the information, Andreas.  If I used an external microcontroller such as a MCU, how would I approach managing multiple IMD devices?  Would I literally switch power on to each unit in turn in a round-robin fashion, switching off all the other units?  Then, the units would be in a perpetual state of doing their poweron measurements, and I would have huge blind spots in the IMD coverage (The Bender IMD boards need at least five seconds after powerup before they can perform their measurements and declare the HV infrastructure safe, so they assume the HV is unsafe - guilty unless proven innocent).  Can you think of a strategy I could use to round-robin IMD boards without suffering measurement dead spots?  In a HV system user safety is paramount, and I don't think this design would be very safe at all.   Any system that is oscillating between safe/unsafe constantly in normal production conditions will be ignored.  Any other suggestions / alternatives you can think of?

  • Hi Myles,

    IMDs are typically not meant to continuously operate. In EV Charging for example the insulation is checked before each charging cycle and then in regular intervals e.g. every minute. 
    For continuous monitoring in a system a GFCI or a RCD is used. These devices check the leakage currents continuously and trip the system as soon as the pass a threshold. For a RCD implementation we have another reference design called TIDA-010237.

    Best regards,
    Andreas

  • It may be instructive to post what ChatGPT4 had to say on the topic:

    1. Insulation Monitoring Device (IMD): An IMD is a device used to monitor the insulation resistance of an ungrounded system between an active phase conductor and earth. It is particularly useful in identifying the first fault in an ungrounded system, which can prevent electrical shock or fire hazards. IMDs are commonly used in healthcare facilities, maritime and offshore installations, and other critical applications where continuity of service is required.

    2. Ground Fault Circuit Interrupter (GFCI): A GFCI is a device that shuts off an electric power circuit when it detects that current is flowing along an unintended path, such as through water or a person. It is used to reduce the risk of electric shock, which can cause the heart to stop or cause burns. They can also prevent some electrical fires by interrupting the flow of electricity in time.

    3. Residual Current Device (RCD): An RCD, also known as a Residual Current Circuit Breaker (RCCB), is a device that instantly breaks an electric circuit to prevent serious harm from an ongoing electric shock. It works by detecting the imbalance of electrical current caused by the leakage current (residual current).

    Now, let's compare and contrast them:

    • Functionality: All three devices are designed to protect electrical systems and their users. However, they do this in different ways. IMDs monitor the insulation resistance of an ungrounded system and alert to the first fault, GFCIs protect individuals from electric shocks from faults in the device or line, and RCDs protect from electric shocks caused by direct contact with live parts and indirect contact with exposed conductive parts.

    • Use Cases: IMDs are used in critical systems where continuity of service is required, such as in healthcare or maritime applications. GFCIs are commonly found in residential and commercial applications, particularly in areas with a higher risk of contact with water. RCDs are used in various environments, including residential, commercial, and industrial, for general shock protection.

    • Operation: IMDs continuously monitor the insulation level of a system and do not interrupt the power supply. On the other hand, both GFCIs and RCDs interrupt the power supply when a fault is detected. However, GFCIs are designed to protect from ground faults, while RCDs protect against residual currents.

    • Protection Level: GFCIs and RCDs provide personal protection against electric shock, while IMDs provide system protection by monitoring the insulation resistance and providing early warning of potential faults.

    Remember, the choice between these devices depends on the specific requirements of the electrical system and the level of protection needed.