Hi Team,
Datasheet shown that our Rtrip range as below :

That said if Rtrip at between 0~3.16K, then the OC point will be 8.1~9A , right?
My question will be if the Rtrip > 30.1K, what will happen ? Is it will limit at a certain current or it can follow below formula?

I asking this question is my customer plan use this part for all those part 0~6A power rail, when small current application such like 0.5A, if they want to protect at 0.7A, it that ok? Such like place a 42.8K Rtrip?
Thanks!
BR,
Kai