This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please recommend cell battery monitoring IC.

Hi

My customer is looking for IC with the following specifications.
Please recommend something.

-SPEC-

Production:  Cell battery Monitor
Cell Configuration: 20S / 3P
Specifications: Supply Voltage  60V over

Thanks

  • Hi David,

    Based off the information you have provided, the BQ7961x-Q1 device family could be suitable for these specs. This is a stackable device, so they can stack the BQ7961x-Q1 devices to meet a 20S requirement. Please note that this device family does not support current measurement.

    If current measurement is necessary, the BQ7965x-Q1 device family could meet that requirement as well (also stackable). 

    Best Regards,

    Julia Louis