What is the ESD (human body model) rating for CSD19502Q5BT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kiran,
Thanks for your interest in TI FETs. The CSD19502Q5BT passes 2250V HBM and 2000V CDM. FYI - the CSD19502Q5B and CSD19502Q5BT are the same FET. The only difference is the reel size and quantity. The CSD19502Q5B is on the large reel with 2500 pieces per reel and the CSD19502Q5BT is on the small reel with 250 pieces per reel.
Best Regards,
John Wallace
TI FET Applications