Hello,
I'm looking into LED Driver to act as a adjustable current source to drive my resistive load.
Can you recommend some ICs which can achieve my requirements please:
1. Load 1: buck-boost configuration
- R = 6,5Ohm
- I = 2,5A
2. Load 2: boost configuration
- R = 400Ohm
- I = 250mA
Input: +12V
Input control signal: DAC output 0..2,5V
Thank you very much in advance.