Hi Team
I am working on a project with BQ76952. I need to give wakeup signal to TS2 and simultaneously measure NTC temperature sensor with TS2. Please guide me if it is possible to use TS2 with two inputs at the same time? And if possible please tell me its circuit. Because currently the wakeup signal is not working. I also need the LD pin for dipper input and can't use it for wakeup.