This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131-Q1: about AEC-Q100 Qualified test

Part Number: TPS65131-Q1
Other Parts Discussed in Thread: TPS65150-Q1

Hi Sir,

The customer asked that TPS65131-Q1 and TPS65150-Q1 both devices if have passed the below AEC-Q100 Qualified test items? or only have passed some test items?

Both devices' D/S showed the "AEC-Q100 Qualified" is determined based on TI's internal test results? Or is it verified by an external company?

Standard

Details

AEC-Q100

Failure Mechanism Based Stress Test Qualification For Integrated Circuits (base document)

AEC-Q100-001

Wire Bond Shear Test

AEC-Q100-002

Human Body Model (HBM) Electrostatic Discharge Test

AEC-Q100-003

Machine model (MM) Electrostatic Discharge Test

AEC-Q100-004

IC Latch-Up Test

AEC-Q100-005

Non-Volatile Memory Program/Erase Endurance, Data Retention, and operational Life Test

AEC-Q100-006

Test of parasitic gate leakage current caused by thermoelectric effect.

AEC-Q100-007

Fault Simulation and Test Grading

AEC-Q100-008

Life cycle failure rate(ELFR

AEC-Q100-009

Electrical Distribution Assessment

AEC-Q100-010

Solder Ball Shear Test

AEC-Q100-011

Charged Device Model (CDM) Electrostatic Discharge Test

AEC-Q100-012

Short Circuit Reliability Characterization of Smart Power Devices for 12V Systems