This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77216: How to select shorted inputs in BQ77216

Part Number: BQ77216
Other Parts Discussed in Thread: BQ76940

I have a battery pack with 8 cells. I have to design a slave board with a battery monitor like BQ769x2 and I want to add also the BQ77216. I must choose which inputs of BQ77216 I have to short to work only with 8 cells instead of 16 supported by the device. Reading the datasheet of BQ77216, in chapter 10.2, there is the following text

"When paring with the BQ769x2 or BQ76940 devices, the top cell must be used"

If I well understand, this means that I must place a cell between V16 and V15?

Do I have some other constrain in choosing the shorted inputs to work with only 8 cells?

Regards

Andrea