In my design Dock station have two ports for external power supply:
The first is Type C charger connected to port B of TPS65988
the second is Standard Power supply with DC jack.
in both cases the Buck 3.3V supply to system VIN_3V3 (pin #5) of TPS65988.
The first question is PP1_cable mandatory? Can I leave this pin floating?
The second question is which hardware strap configuration in pin ADCIN1_BUSPOWER (#36) I should implement to right boot?
I actually have two cases.
The system can be powered from an external supplier as a self-powered device.
And sometimes the system needs to be powered from the B (Sink) port of the TPS65988 using an external type-C charger.
Port A is UFP and source (5V - 20V@3A) only that connected to notebook.
Thanks in advance