Other Parts Discussed in Thread: LM5156EVM-BST
Hi Team,
I have a question about Demoboard LM5156EVM-BST.
now, I try to change the voltage IC with Demoboard LM5156EVM-BST,
testing condition is
>Input voltage 12V,
>Output voltage 25V
>Fsw=2200kHz
>I Out;30mA
then, I modify the testing board as below,
>Inductor 22μH
>Cout =4.7μF×2, and 10μF×2
*FET and Diode is original (not changed to demoboard).
Then, as test result of current measurement.
current amount of Inductor's output is IRMS=182mA, IMAX=231mA (attached)
so, this amount is much larger than calculation result by the below fomula. (calculation result is I MAX=141mA)
please let me know your advice about difference between calculation result and test result.