Other Parts Discussed in Thread: LM61460EVM, LM61460
Hello expert,
Output 7V 5A, we connect the output load 1.5R first and than we supply the Vin with 9V 13.5V or 16V, we test the waveform from En pull high to output voltage establish.We find two issue:
1.response time too long, when En is high,it take about 20ms for this device to react and start to ramp up the output voltage.
2. output drop to 4.2V for about 25ms and then recover to 7V.

we remove the output 1.5R load and redo the test, the question1 is the same,and the question 2 the voltage drop is some what better.

Pls tell me how to improve this issue,thank you!