This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS564247: Output Current

Part Number: TPS564247
Other Parts Discussed in Thread: TPS566247, TPS565247

Hello,

This device is advertised as a 4A device, but the recommended operating conditions list the max output current as 6A. Can this device operate up to 6A or is that a typo?

Also, on the first page of the datasheet it says "Part of a full P2P family including solutions for 4 A, 5 A, and 6 A and FCCM/ECO operation." Is the 6A version released?

Thanks,

Michael