This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LV2862: Minuscule Audible noise

Part Number: LV2862
Other Parts Discussed in Thread: LMR51606

Hi,

I have tried our first prototypes and output seems to be regulating well for our load which is a average load of ~7mA with peak loads of ~18mA for a duration of ~10ms.

We use the 770kHz fsw.

When I measure the output ripple, it is about 15mV @ 10kHz. I wonder if it is this 10kHz that is audible. 

How can I suppress this noise?

Cheers,

Kaushalya