Other Parts Discussed in Thread: LM5170, UCD3138, LM5176
Hi, TI's expert:
I used a single LM5175 chip for 20V ,8A output design and it works well.
But now, I need design a 3600W output rating power, the output voltage is 24V and 48V(both need be met).
which means the design should afford more than 150A(75A in 48V output) current . so my iissue is , can the LM5175 use in parallel ?
if can use in parallel, like, I can parallel it with 8 lanes, then, the current less than 20A in single LM5175.