This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: I'm wondering the LM5175 chip can use in parallel for a 3.5KW output

Part Number: LM5175
Other Parts Discussed in Thread: LM5170, UCD3138, LM5176

Hi, TI's expert:

   I used a single LM5175 chip for 20V ,8A output design and it works well.

   But now, I need design a 3600W output rating power, the output voltage is 24V and 48V(both need be met).

   which means the design should afford more than 150A(75A in 48V output) current . so my iissue is , can the LM5175 use in parallel ?

   if can use in parallel, like, I can parallel it with 8 lanes, then, the current less than 20A in single LM5175.