Other Parts Discussed in Thread: TPSM63610,
Hi support team,
The TLVM13610 does not have a MODE pin like the TPSM63610.
Is there a way to make it FPWM at light load?
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Dice,
As I know the difference between the two part is "VOUT range" and "with or without SPREAD SPECTRUM", looking from the pin table the pin 15 could not pull High to enable FPWM, but on plot page it have the efficiency data,
Let me check with device owner whether this function is disabled or not.
Elena
hi, Dice,
The TLVM13610 is set to PFM only. The pin table description is right .
The FPWM mode curves might have been copied from the TPSM63610 datasheet but not filtered out for the TLVM13610.
If you need FPWM, please use the TPSM63610 which has the SYNC/MODE pin.
Elena