This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22680: LM22680QMRE-ADJ/NOPB Webench simulation

Part Number: LM22680


Hi,

I was using the Webench tool to simulate LM22680QMRE-ADJ/NOPB with the following inputs

  1. Vin(min) - 22V
  2. Vin(max) - 24V
  3. Vout - 12V
  4. Iout - 2A

But the webench gives a design fail popup.

Could anyone explain me the reason?

Regards,

Hareesh