Other Parts Discussed in Thread: BQ27410-G1, BQ27220
Hellow.
The BQ27410-G1 is used with the structure shown below.

It outputs the SOC value normally at idle (0.8A).
Active (1.3A) normally outputs the SOC value, but it suddenly greatly decreases.
After restarting again, there is a problem with returning to the original value.
<SOC value(Active)>
1min: 100%
2min: 98%
3min: 96%
4min: 94%
5min: 92%
6min: 60%
Restart(offàon): 90%
Thank you.