Hi Team,
Please help check schematics and project condition, Vin24~28V@0.5A to 3.3V@0.2A

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Please help check schematics and project condition, Vin24~28V@0.5A to 3.3V@0.2A

Hi Kevin,
Thanks for reaching to us!
Actually many items in schematic need to be optimized. My comments are listed below.
1. EN-pin max absolute voltage is 6V, cannot pull EN-pin directly to 28Vin.
2. Suggest 0.1uF boot cap, 1nF is too small.
3. Suggest to add a 0.1uF input decoupling cap as close to IC as possible.
4. Only 1uF output cap is not enough. Please refer to datasheet reference schematic and LC recommended table.