Part Number: TPS2521
Hello,
I have a question regarding the junction temperature of the TPS2521.
The maximum rating of TJ is described as "Internally Limited", but what is the actual temperature?
Thermal shutdown is 154°C. lower than that?
If it is low, the maximum rating will be exceeded if thermal shutdown is activated.
Will the device then be destroyed?
If destroyed, what symptoms of destruction are expected?
Best regards,