This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need a watchdog with Chip Enable/Watchdog disable and Latching output

Hello,

I need help finding a watchdog part with the below features.

  1. Chip Enable or Watchdog Disable: To disable the watchdog during start-up.
  2. Latching Output
  3. Output type can be either Push-Pull or Open-Drain
  4. Active low output preferred

Regards