Hello,
I have a project where I need a USB-UART Bridge (CP2102N-A02-GQFN28) to program and communicate with the MCU over USB. In a second project I use a MCU (ESP32-S3) with integrated USB functionality. In both cases I want the BQ25895M, but I am pretty sure that the USB datalines of the two devices cannot be mereged that easily. Can please someone explain how to do that :-)
Best regards from Germany!