Part Number: LM5116
Hi,
I have designed a boost converter with the help of WEBBENCH. The result is as follows: https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=0849EFBB2C4F6E22
My Requirement is to get 24V/15A MAx output from a 48 V Source (Min I/P: 35V, Max I/P: 60V).
Please verify my attached schematics. Also, I have some queries, while exporting the output from Webbench to altium, I found some components are not in schematics but were there on layout. Can you please explain them:
1. There is an R-Ramp across ramp pin on PCB but not in schematics.
2. One diode is connected between UVLO (Pin 2) and VIn. Is it mandatory?
3. There is a C Sync capacitor on C SYnc pin and it is not there on schematics.
4. What is R Snub and C Snub. How to connect them in schematics. Is it mandatory?
5. What is D3 and NT1 connected between SW Pin and HB Pin?