Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25622EVM: Via size

Part Number: BQ25622EVM

Hello,

In the Datasheet there is a recommendation to place some vias under the IC to route the SW node with the inductor. 

If I check the Board Layout I see that there are 8 vias under the IC for this purpose and also 3 extra vias for GND.

What is the size of those vias (drill + pad) so the board is manufacturable without being so expensive?

What is the correct number of vias to be placed related to their drill size? (in case a must use a different via size than TI's)

Could you please share the size of the power vias ?

Is it mandator to route a copy of the Top Power Plane on the bottom side? My board will use 2A

How many vias should I place and which size should they be?

Thank you