Other Parts Discussed in Thread: LM61440
Hello expert,
Input 9~16V,output 7V 5A,power coil is 4.7uH,below is the schemitic
I want to test the output over current limit function of this device. But when I increase the Eload CC current from 5A to 6A and then 7A,the BUCK is still working on 7V 7A. Is seems that no current limit function.Can you confirm?
And if no current limit on this device, how to ensure the safety when output load is over current?