This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB-PD-CHG-EVM-01: Connection failure with TPS25750EVM

Part Number: USB-PD-CHG-EVM-01
Other Parts Discussed in Thread: TPS25750EVM, TPS25750

Hi support team.

I'm trying to connect USB-PD-CHG-EVM-01 and TPS25750EVM.

USB-PD-CHG-EVM-01 is source(27W/9V) ,TPS25750 is sink.

After configuring each one and connecting, they start negotiating and establish once, but then repeat the negotiation.

The output on the source side also outputs 9V, but it is turned off immediately and started again.

Please refer to the attached document for details.

I also monitored the current on the source side, but the current over the current limit is not flowing.

Could you help me find out what is causing this?

Best regards,

Higa


TPS25750 connection issue.pdf