This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481-Q1: Output ripple is present in the reference design generated in webench

Part Number: LM3481-Q1
Other Parts Discussed in Thread: LM3481,

hi,

I was working on a aux power supply for an automotive application, so I decided to generate a boost PS solution with LM3481 Q1 with webench. My input is a varying DC source from 9VDC to 16VDC and output is fixed 20VDC with a current of 0.5A total power is 10W and operating frequency is 200kHz.the design suggested from webench having a lot of ripple present at the output which is even available in their simulation tool it self. Can anyone help me with this matter? With low ESR distributed capacitors, I have been able to reduce the ripple to 7mVpp; however, the ripple frequency and shape remain the same.