Hi team,
The customer wants to wake up the MCU by interrupting the MCU through the alert pin. When exiting sleep, the alert pin signals an interrupt, but after exiting and entering sleep, the alert pin always outputs a high level with no change in signal.
The alert pin config is set as shown in the figure below, the alert pin is connected to 3.3V as recommended by the EVM with 10k pull-up:
Could you help check this case? Thanks.
Best Regards,
Cherry