Other Parts Discussed in Thread: BQ76952, , EV2400
Hi team,
The BQ76952 and BQ76200 are directly connected. The battery is a 48-V system. When these two devices are connected, approximately what is the high level of DSG_EN,CHG_EN? Could you help share some test waveforms?
When customers use the power supply to test these two signals, they will increase with the battery voltage. Connect to EV2400 control, VBAT is 30V, DSG_EN and CHG_EN signal are approximately 20V. BQ76200 output is abnormal. CHG, DSG signals are small duty cycle switching signals. Here is the schematic:

Could you help check this case? Thanks.
Best Regards,
Cherry