Other Parts Discussed in Thread: EV2400
Hi team,

Issue: The switch section does not work, and 2 boards are the same problem. But the 6 V of REGN is good. The customer is trying to capture the G-pole waveform of the MOS at the beginning of power up, but there are no waveforms. Measured pin voltages are as follows:
VBUS=12V,SW1=SW2=1.1V,BTST1=BTST2=5.42V,HIDRV1=HIDRV2=1.1V,LODRV1=LODRV2=0V.REGN=5.75V
Could you help check this case? Thanks.
Best Regards,
Cherry