This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: chemistry ID

Part Number: BQ40Z80

Hi team,

The battery is marked with a capacity of 1500 mAh and a full charge of 4.2 V. A discharge current of 0.1C is required to make the chemistry ID, i.e. 150mA discharge to 3V cut off voltage. The actual discharge time is about 6h, but it should theoretically be close to 10 hours. Will there be an error in the chemistry ID measured this way? Is it required to reduce the discharge current to ensure the discharge time is close to 10 hours? 

Below is a report of 150mA discharge current for chemistry ID:

Chemistry ID selection tool, rev=2.54		
		
Configuration used in present fit:		
ProcessingType=2		
NumCellSeries=1		
ElapsedTimeColumn=0		
VoltageColumn=1		
TemperatureColumn=2		
CurrentColumn=3		
		
Best chemical ID : 3717	Best chemical ID max. deviation, % : 1.85	
		
		
		
Summary of all IDs with max. DOD deviation below 3%		
		
Chem ID	max DOD error, %	Max R deviation, ratio
3717	1.85	0.16
2684	1.98	0.19
2021	2	0.44
5691	2.04	0.5
1211	2.04	0.26
204	2.11	0.43
1320	2.15	0.44
106	2.21	0.11
2582	2.22	0.24
5432	2.22	0.48
2005	2.23	0.13
1139	2.24	0.05
1343	2.26	0.22
260	2.28	0.78
3607	2.28	0.53
5267	2.29	0.09
3720	2.3	0.71
1151	2.3	0.07
2022	2.33	0.31
113	2.4	0.48
1223	2.43	0.25
1270	2.46	0.05
250	2.46	0.07
5220	2.48	0.09
5605	2.49	0.13
2064	2.5	0.95
281	2.51	0.03
181	2.52	0.06
1110	2.53	0.15
2987	2.54	0.23
2459	2.56	0.76
1154	2.58	0.47
2274	2.59	0.18
1309	2.62	0.42
1348	2.62	0.28
257	2.64	0.1
528	2.65	0.02
2108	2.67	0.57
2404	2.67	0.02
234	2.69	0.04
235	2.71	0.04
1976	2.73	0.52
1128	2.74	0.04
2702	2.76	0.05
264	2.81	0.05
2148	2.83	0.01
1241	2.83	0.06
258	2.84	0.02
1204	2.85	0.64
2143	2.88	0.28
285	2.88	0.08
1341	2.89	0.13
5345	2.9	0.09
1243	2.91	0.09
2011	2.93	0.24
1217	2.93	0.09
5379	2.94	0.22
2129	2.94	0.22
2128	2.95	0.02
101	2.97	0.77
2040	2.99	0.04
2153	2.99	0.05
243	2.99	0.13
		
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.		
		
		
Selection of best generic ID for ROM based devices like bq274xx		
		
		
Device / Family #1		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
128	bq27421-G1A: 4.2V LiCoO2	3.39
354	bq27411-G1C: 4.35V LiCoO2	3.78
312	bq27421-G1B: 4.3V LiCoO2	3.83
3142	bq27421-G1D: 4.4V LiCoO2	3.94
Best generic ID 128		
Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
		
		
Device / Family #2		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
1210	bq27621:  (ALT_CHEM1) 4.3V LiCoO2	3.37
1202	bq27621: (default) 4.2V LiCoO2	3.49
354	bq27621:  (ALT_CHEM2) 4.35V LiCoO2	3.78
Best generic ID 1210		
Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
		
		
Device / Family #3		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
3230	bq27426: (default) 4.35V LiCoO2	3.48
1202	bq27426: (ALT_CHEM1) 4.2V LiCoO2	3.49
3142	bq27426: (ALT-CHEM2) 4.4V LiCoO2	3.94
Best generic ID 3230		
Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.		
		
		
Warning: Discharge rate is too high. High rate reduces ID detection accuracy	 10 hr rate is recomeended. Total discharge time is less than 5 hrs	 t_hrs=  2.78906527777778

Could you help check this case? Thanks.

Best Regards,

Cherry