This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55289: Level shift for I2C and enable pin

Part Number: TPS55289


Hello,

Does this interfaced works or does it require a level shifting? The I2C lines are going directly to a micro controller that is working at 3.3V and the TPS55289 is configured to use internal LDO. So I was wondering if I need to shift that voltage level for I2C pins and also for enable pin?

Regards,

Khan