This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Asking for LDO design review and suggestions

Hi Team,

Customer would like to design LDO for Vin 3V cases.

Would you please review the Vout/Iout requirement here and provide recommendations?

Fixed output is prefer.

 

Vout: 1.29V (1.27~1.31)

Iout: 137mA

 

Vout: 0.95V (0.92V~0.98V)

Iout: 650mA

 

Vout: 1.2V (1.15V~1.32V)

Iout: 613mA

Thanks for help!

 

SHH

  • Hello,

    My recommendations are the following:

    Vout: 1.29V (1.27~1.31)

    Iout: 137mA

    TLV70313DBVR

    Vout: 0.95V (0.92V~0.98V)

    Iout: 650mA

    TPS7A7401DSDR  - Needs bias rail and is adjustable, we do not have fixed voltages for 0.95V in our portfolio.

    Vout: 1.2V (1.15V~1.32V)

    Iout: 613mA

    TLV75712PDRVR - Thermals might become an issue here

    Regards,

    Andres